AIN#.DEADBANDMODE
Description
When AIN#.DEADBANDMODE is set to 0, and the value of the analog input is less than the absolute value of AIN#.DEADBAND, the analog command will be 0. When the analog input is greater or equal to the absolute value of AIN#.DEADBAND, then the analog command will be generated using the scaling specified.
When AIN#.DEADBANDMODE is set to 1, the analog command is 0 if the input is less than the absolute value of the deadband value. When the input is greater than the absolute value of the deadband, the output is equal to (Input - Deadband) * Scaling.
Below are illustrations of this behavior.
Examples
Context
For more information see Analog Input.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read/Write |
| Units | N/A |
| Range | 0 to 1 |
| Default Value | 0 |
| Data Type | Integer |
| See Also | |
| Stored in Non Volatile Memory | Yes |
Variants Supported
All variants are supported.